Curve Selection and Color Table

Velocity (first derivative), acceleration (second derivative) and jerkIn physics, jerk is the rate of change of acceleration; more precisely, the derivative of acceleration with respect to time (third derivative) plots are displayed in the lower graph. If the element is a line, the velocity is constant and acceleration is 0.

With the check boxes in the Curve selection table shown in figure below, you can select or clear each individual curve to be displayed.

When a curve is selected (see blue highlighted row in figure below), the Y-scale of the Curves graph is adjusted to display the Y-scale of the selected curve. Also, the color of the 'tick' line of the scale is changed to match the color code of the selected curve.

Curve Selection Table

Figure 10-14: Curve Selection Table

How to change color

You can change the color of a plot as follows:

  1. Double-click on a colored square shown in the Curve Selection Table to open the color selection dialog box
  2. Standard Color Selection

    Figure 10-15: Standard Color Selection

  3. Click on an existing color square to select it, or specify the numerical values for a color. (You can also move the black indicator on the right side until the desired color appears in the large colored rectangle)

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™